Beli Thermometer Gp Care di monotaro.id
Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
- FOSROC Conbextra GP Cementitious Grout (Semen Pengisi Celah)Deskripsi:Conbexlra GP general purpose non-shrink cementitious grout, is supplied as a ready lo use dry powder. The addition of a controlled amount of clean water produces a fowing non-shrink grout for gap thicknesses up to 100 mm. Conbextra GP is a blend of Porliand cement, graded fllers and chemical additives which impart controlled expansion in the plastic state whilst minimising water demand. The low wate rdemand ensures high early strength. The graded tiller is designed to assist uniform mixing and produce a consistent grout. Uses. Conbexlra GP is used for general purpose grouling where it is essenlial to eliminate shrinkage when completely Filling the void between a base plate and a substrate. Such an applicalion would be the grouting of a stanchion base plate. It can also be used roF anchoring a wide range of Fixings. These include masts, anchor bolts and fence posts. Advantages. - Gaseous expansion system compensates tor shrinkage and setllement in the plastic stale. - No metallic iron content to cause slaining. - Pre-packaged material overcomes potential on-site botching variations. - Develops high early strength without the use of chlorides. - High ultimate strength and low permeability ensure the durability of the hardened grout. Technical support. Fosroc offers a comprehensive range of high quality, high performance conslruction products. In addition, Fosroc ofers a worldwide technical support and on-site service to specifiers, end-users arid contractors. Supplier specification. All grouting where shown on Ihe drawing must be carried out using Conbextra GP manufactured by Fosroc and used in accordance with the manufacturer's data sheet. Application instructions. Foundation surface. The substrate surface must be free from oil, grease or any loosely adherent material. If the concrete surface is defective or has lailance, fl must be cut back to a sound base. Bolt holes and fixing pockets must be blown clean of any dirt or debris. Pre-soaking. Several hours prior to grouting the area of cleaned foundation should be flooded with fresh water. Immedialoly before grading takes place any free water should be removed with particular care being taken ID blow out all bolt holes and pockets. Base plate. It is essential that this is dean and free from oil, grease or scale. Air pressure relief holes should be provided to allow venting of any isolated high spots. Levelling shims. If these are to be removed after the grout has hardened, they should be treated with a thin layer of grease. Formwork. The formwork should be constructed to the leakproof. This can be achieved by using foam rubber strip or mastic sealant beneath the constructed formwork and between joints. In some cases it is practical to use a sacrificial semi-dry sand and cement formwork. The formwork should include outlets for pre-soaking. Unrestrained surface area. This must be kept to a minimum. Generally the gap width between the perimeter formwork and the plate edge should not exceed 150 mm on the pouring side and 50 mm on the opposite side. It is advisable where practical to have no gap at the fank sides.atribut:
- Consistency Yield (L): Trowellable 12, Flowable 13.25
- IRC Motorcycle Tyre Tubeless (Ban Luar Motor)Deskripsi:Desain telapak ban yang kokoh dan elegan dengan fungsi kenyamanan berkendara yang optimal pada saat traksi, pengereman dan manuver di jalan
- Fenix SenterDeskripsi:FenixC6 V3.0 adalah lampu kerja isi ulang berkinerja tinggi, yang dirancang khusus untuk perawatan dan perkerjaan industri umum, seperti perbaikan mobil, patroli malam, memperbaiki sirkuit listrik, dan sebagainya. Magnet di bagian ekor mudah untuk anda tempelkan ke permukaan logam, memberikan penggunaan hands-free. Selain itu, dua mode hadir dengan enam output yang dioperasikan oleh satu tombol, menawarkan pencahayaan optimal di setiap lokasi kerja. Didukung oleh baterai Li-ion 18650 2600mAh yang dapat diisi ulang. FenixC6 V3.0 membantu anda menyelesaikan pekerjaan dalam keadaan apa pun.Kelengkapan:FenixC6 V3.0 flashlight x1FenixARB-L18-2600 rechargeable Li-ion battery x1USB C-Type charging cable x1Lanyard x1Spare O-Ring x1User manual x1
- FOSROC Nitoflor Hardtop Floor Hardener Natural (Lapisan Permukaan Beton)Deskripsi:Monolithic surface hardening compound for fresh concrete floorsNitoflor Hardtop surface hardening compound is a quality controlled, factory blended powder which is ready to use on site. It consists of special hard wearing aggregates selected for their physical properties of abrasion and wear resistance, Portland cement and special additives to improve workability.This combination produces a material Nitoflor Hardtop cures monolithically to provide a dense, non porous surface which is extremely hard wearing and abrasion resistant. Monolithic cure ensures that problems normally associated with thin ('granolithic') screeds, e.g. curling, shrinkage, cracking, etc. are completely overcome. Nitoflor Hardtop is available in natural (concrete grey) colour as standard. Special colours, including Brick Red and Green can be produced on request for large orders.UsesNitoflor Hardtop provides a highly abrasion resistant surface to fresh concrete foors by the dry shake method which ensures that the hard wearing surface bonds monolithically to the base concrete. It is ideally suited for all industrial areas subjected to heavy trafic, e.g. power stations, heavy industry, breweries, agricultural buildings, distillation plants, laboratories, abattoirs, warehouse floors, loading bays and work shops.Advantages- Supplied ready to use - no additives required- Provides a hard, abrasion resistant surface- Forms monolithic bond with fresh concrete base- Hard, dense surface resistant to oils and grease- Available in a range of colours to improve working environment- Non-metallic aggregate - will not rust when wetTechnical support Fosroc ofers a comprehensive range of high performance, high quality fooring, jointing and repair products for both new and existing foor surfaces. In addition, Fosroc ofers a technical support package to specifiers, end-users and contractors, as well as on-site technical assistance in locations all over the world.Base concreteThe base concrete should have a minimum cement content of 300 kg/m3. The concrete mix should be designed to minimise segregation and control bleeding, although some limited bleed is desirable to ensure sufficient moisture is available to wet out the Nitoflor Hardtop when it is first applied. The use of water reducing admixtures from the Fosroc Conplast* range is strongly recommended in order to achieve a water:cement ratio below 0.55. The base concrete should have an on-site slump of between 75 and 100 mm. The base concrete should be laid and compacted in accordance with good concrete practice, taking care to ensure accurate finished profile and minimum laitance build up. Particular attention should be paid to bay edges and corners to ensure full compaction of the base concrete - see application instructions. Vacuum dewatering is not recommended.atribut:
- Size (kg): 25
Daftar Harga Thermometer Gp Care Terbaru October 2026
| FOSROC Conbextra GP Cementitious Grout (Semen Pengisi Celah) | Rp139.900 |
| IRC Motorcycle Tyre Tubeless (Ban Luar Motor) | Rp199.900 |
| Fenix Senter | Rp289.900 |
| FOSROC Nitoflor Hardtop Floor Hardener Natural (Lapisan Permukaan Beton) | Rp119.900 |
Data diperbarui pada 10/10/2026 (Harga belum termasuk PPN)



















































































































































/lqP105308782-2.jpg)
/P103100618-1.jpg)

/n6P105308834-1.jpg)
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
/WD-40%20Multi-Purpose%20Lubricant%20(Pelumas%20Serbaguna)%20333ml%201pc/60S000055216-2.jpg)
/OLFA%20Cutter%20Knife%20Safety%20(Pisau%20Cutter)%20149B%201pc/S009054721-2.jpg)
/Joyko%20Gel%20Ink%20Pen%20Q%20(Pulpen%20G2%20%2F%20Pulpen%20Gel)%20GP-265%20Black%200_5mm%201box(12pcs)/qmS009904958-2.jpg)
/REXCO%20Multi-Purpose%20Lubricant%20(Pelumas%20Serbaguna)%20RX-SP0009%20500ml%2F415g%201pc/2bS000076083-4.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Sarung%20Tangan/Sarung%20Tangan%20Tahan%20Minyak/Sarung%20Tangan%20Tahan%20Minyak%20Karet%20Nitril/ANSELL%20Gloves%20Solvex%20Nitrile%20(37-176)%20(Sarung%20Tangan%20Nitrile%20Anti%20Kimia)/ANSELL%20Gloves%20Solvex%20Nitrile%20(37-176)%20(Sarung%20Tangan%20Nitrile%20Anti%20Kimia)%2037-176%20Size%209%201pair/S000074366-1.jpg)

%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)/IKA%20(Copy%20Paper)%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20IKF%20PC%2070%20A4G%201ream/8pS035166313-2.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Kesehatan/Pertolongan%20Pertama%2C%20Kebutuhan%20Higienis/Perban%2C%20Kain%20Kasa/OneMed%20Alkohol%20Swab%20(Tisu%20Alkohol)/OneMed%20Alkohol%20Swab%20(Tisu%20Alkohol)%201box(100pcs)/h6S039287618-2.jpg)
/3M%20Post-it%20654%20Sticky%20Notes%20(Kertas%20Memo)%20654-5CY%201pack(5pads)/5iS030245198-4.jpg)
/monotaro_id%20Lakban%20OPP%202inch%20(Solasi%20%2F%20Selotip)%20Transparent%2048mmx64m%201roll/h7S036166619-4.jpg)

/monotaro_id%20Cable%20Ties%204_8x250mm%20(Pengikat%20%2F%20Kabel%20Tis)%20White%201pack(100pcs)/2xS039549105-2.jpg)
/Max%20Stapler%20Needle%20(Isi%20Staples)%20No_10-1M%205%2F16x3%2F16Inch%201pack(20pcs)/S000005230-4.jpg)
/monotaro_id%20Plas%20Chamois%20(Lap%20Kanebo)%20with%20tube%20Yellow%2032x21cm%201pc/4uS037754174-2.jpg)